Version History
The following information lists the changes that were introduced in each tool release:
Release 8
Release name: Power Monitoring Expert - Configuration Manager 2022
Release date: August 2022
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
(Exception: PME 8.1 archives created with Configuration Manager 2.0.1 can be loaded and written.)
System support
| Server or Machine | Version |
|---|---|
| Source |
PME 7.2.2 |
| Target | PME 2022 |
NOTE: Upgrades and migrations between different architectures are also supported (Standalone -> Distributed Database, Distributed Database -> Standalone)
New features
- Support for all localized versions of PME.
Release 7
Release name: Power Monitoring Expert - Configuration Manager 2021
Release date: May 2021
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
(Exception: PME 8.1 archives created with Configuration Manager 2.0.1 can be loaded and written.)
System support
| Server or Machine | Version |
|---|---|
| Source | PME 7.2.2 PME 8.2 PME 9.0 PME 2020 PME 2021 |
| Target | PME 2021 |
NOTE: Upgrades and migrations between different architectures are also supported (Standalone -> Distributed Database, Distributed Database -> Standalone)
New features
- Support for all localized versions of PME.
Release 6
Release name: Power Monitoring Expert - Configuration Manager 2020
Release date: Nov 2019
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
(Exception: PME 8.1 archives created with Configuration Manager 2.0.1 can be loaded and written.)
System support
| Server or Machine | Version |
|---|---|
| Source | PME 7.2.2 PME 8.2 PME 9.0 PME 2020 |
| Target | PME 2020 |
NOTE: Upgrades and migrations between different architectures are also supported (Standalone -> Distributed Database, Distributed Database -> Standalone)
New features
- Support for upgrades and migrations between different architectures.
Release 5
Release name: Power Monitoring Expert - Configuration Manager 9.0
Release date: Aug 2018
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
(Exception: PME 8.1 archives created with Configuration Manager 2.0.1 can be loaded and written.)
System support
| Server or Machine | Version |
|---|---|
| Source | PME 7.2.2 PME 8.2 PME 9.0 |
| Target | PME 9.0 |
NOTE: Only upgrades and migrations within the same architecture are supported (Standalone -> Standalone, Distributed Database -> Distributed Database)
New features
- Support for all PME Editions.
- Support for all localized versions of PME.
Release 4
Release name: Power Monitoring Expert - Configuration Manager 2.1.0
Release date: April 2017
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
System support
| Server or Machine | Version |
|---|---|
| Source | ION Enterprise 6.0.1 PME 7.2.2 PME 8.2 |
| Target | PME 8.2 |
NOTE: Only Standalone system architectures are supported, except for ION Enterprise 6.0.1 Distributed Database systems, which can be upgraded to PME 8.2 Distributed Database.
Release 3
Release name: Power Monitoring Expert - Configuration Manager 2.0.0
Release date: August 2016
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
System support
| Server or Machine | Version |
|---|---|
| Source | ION Enterprise 6.0.1 PME 7.2.2 PME 8.1 |
| Target | PME 8.1 |
NOTE: Only Standalone system architectures are supported.
New features
- Support for migrating historical data.
- Support for more configurable items.
Release 2
Release name: Power Monitoring Expert - Configuration Manager 1.1.0
Release date: April 2015
NOTE: Archived configurations saved with an earlier version of the Configuration Manager are not compatible with this release of the tool.
System support
| Server or Machine | Version |
|---|---|
| Source | PME 7.2.2 |
| Target | PME 7.2.2 |
NOTE: Only Standalone system architectures are supported.
New features
- Adding Notes to a Configuration.
- Adding Attachments to a Configuration.
- Smart Disk Space warns you when free disc space is low.
Improvements
General
- Archive file path and name length can be any length; it is no longer restricted to 256 characters.
- Improved error messaging.
- ETL sources are read, saved, and written as historical sources.
- WebReach Start-up diagrams and Vista start-up diagrams are now supported.
- A hierarchy is always written to the target system, even if it contains broken device references.
User Interface
- Improved messaging and workflows to indicate when services are stopped and restarted.
- Renamed the 'Diagrams' configuration component to 'Customized Diagrams' to better convey that the tool reads and writes new and edited diagrams only.
- Improved tool workflows when operations are completed or canceled.
- The Configuration Manager now displays the Report Subscription's description field:
- Log pane – Added more detail to log messages and improved log message wording.
- Log pane – Changed the default initial sort to show newest log messages first.
Reports
- Reports that were deleted from Custom Report Packs are no longer imported into the target system.
- Default report sharing is supported.
Release 1
Initial release.
Release name: Power Monitoring Expert - Configuration Manager 1.0.0
Release date: November 2014
System support
| Server or Machine | Version |
|---|---|
| Source | PME 7.2.2 |
| Target | PME 7.2.2 |
NOTE: Only Standalone system architectures are supported.