PME release history
The following table lists the major releases of PME. Service pack and hot fix releases are not included in this list.
| PME Name and Version | Year of release |
|---|---|
| Power Monitoring Expert 2023 | 2023 |
| Power Monitoring Expert 2022 | 2022 |
| Power Monitoring Expert 2021 | 2021 |
| Power Monitoring Expert 2020 | 2019 |
| Power Monitoring Expert 9.0 | 2018 |
| Power Monitoring Expert 8.0 | 2015 |
| Power Monitoring Expert 7.2 | 2013 |
| StruxureWare Power Monitoring 7.0 | 2012 |
| ION Enterprise 6.0 | 2009 |
| ION Enterprise 5.6 | 2007 |
| ION Enterprise 5.5 | 2004 |
| ION Enterprise 5.0 | 2003 |
| ION Enterprise 4.5 | 2002 |
| ION Enterprise 4.0 | 2002 |
| ION Enterprise 3.0 | 2001 |
The following table shows the support status for recent PME releases.
| Release | Year | Status | Support Timeline |
|---|---|---|---|
| PME 2022 | 2022 | Full Support | (*) Full Support will end on December 31, 2024 (**) Limited Support will end on December 31, 2026 |
| PME 2021 | 2021 | Full Support | Full Support will end on December 31, 2023 Limited Support will end on December 31, 2025 |
| PME 2020 | 2019 | Limited Support | Full Support ended on December 31, 2022 Limited Support will end on December 31, 2024 |
| PME 9.0 | 2018 | Limited Support | Full Support ended on December 31, 2021 Limited Support will end on December 31, 2023 |
| PME 8.2 | 2017 | Limited Support | Full Support ended on December 31, 2020 Limited Support will end on December 31, 2022 |
| PME 8.1 and earlier | 1992 - 2016 | Mature | Full and Limited Support ended. Recommended to upgrade to latest release. |
(*) Full Support:
- Technical investigation and assistance for issues, including creation of critical hotfixes where deemed necessary by the factory.
(**) Limited Support:
- Answering technical questions.
- Providing workarounds and fixes for known problems, when possible. No hotfixes for new issues.
- Providing information on migration to a newer product release with Full Support.