IIS Application Pools
The Power Monitoring Expert installer enables and configures IIS to host the different Web applications. The following table lists the application pools and applications:
| Application Pool | Identity | Application |
|---|---|---|
| Application Modules App Pool | NetworkService * |
Dashboards EWS (EcoStruxure Web Services) Slideshow System Data Service Web |
| ION App Pool | NetworkService * |
ION ION Report Data Service Web Services |
| Web Reporter App Pool | NetworkService * |
ModelingConfig reporter |
* When PME is installed with Windows Integrated Authentication, then the Windows account that is used to access the database, is also used to run the IIS Application Pools, instead of the Local System account.
NOTE: The .NET Trust Level for PME web applications and Default Web Site must be set to Full (internal), in IIS Manager.