SQL Server accounts
The database server hosts several databases for
For installations with SQL Server Authentication:
| Login | Authentication | Server Role | Database | Membership |
| AMUser | SQL | Public | ApplicationModules | AMApplicationRole |
| ION | SQL | Public | ApplicationModules | db_owner |
| ION_Data | db_owner | |||
| ION_Network | db_owner | |||
| ION_SystemLog | db_owner | |||
| ionedsd | SQL | Public | ION_Data | ION_DSD_Reader |
| ION_Network | NOM_DSD_Reader | |||
| IONMaintenance* | Windows | Public | ApplicationModules | db_backupoperator, db_ddladmin, Maintenance |
| ION_Data | db_backupoperator, db_ddladmin, Maintenance | |||
| ION_Network | db_backupoperator, db_ddladmin, Maintenance | |||
| ION_SystemLog | db_backupoperator, db_ddladmin, Maintenance |
* This account is only created on standalone servers where the SQL Server software and PME are installed on the same computer.
For installations with Windows Integrated Authentication:
| Login | Authentication | Server Role | Database | Membership |
| Account used for Windows Integrated Authentication | Windows | Public | ApplicationModules | db_owner |
| ION_Data | db_owner | |||
| ION_Network | db_owner | |||
| ION_SystemLog | db_owner | |||
| IONMaintenance * | Windows | Public | ApplicationModules | db_backupoperator, db_ddladmin, Maintenance |
| ION_Data | db_backupoperator, db_ddladmin, Maintenance | |||
| ION_Networks | db_backupoperator, db_ddladmin, Maintenance | |||
| ION_SystemLog | db_backupoperator, db_ddladmin, Maintenance |
* This account is only created on standalone servers where the SQL Server software and PME are installed on the same computer.
NOTE: When PME is installed with Windows Integrated Authentication, the Windows account that is used to access the database is also used to run the PME services and the IIS Application Pools.
Other
PME must have access to the master and tempdb System Databases.
The PME Database Manager tool requires that the Windows account that is used to run it has sysadmin permissions on the PME SQL Server instance. The Database Manager is an optional tool, used for managing the PME databases.