Components
The DDD Indicators application is based on the following system components and features:
- Power Monitoring Expert 2023 software.
- Power monitoring devices with Disturbance Direction Detection (DDD) functionality. (See Prerequisites for a list of compatible devices.)
- A one-line diagram of your electrical network.
- A Virtual Processor (VIP) framework.
NOTE: Creating the basic one-line diagram, without indicators, is outside the scope of this application description. For information on how to create diagrams in PME, see Creating and customizing a user diagram.