Prerequisites
The following is required to set up the Thermal Monitoring of LV Busways application in PME:
- PME must be installed and commissioned.
- The busway temperature sensors must be connected to the ZBRN32 access point and must be communicating.
- The ZBRN32 access point must be connected to an Ethernet Gateway, such as the Link150.
- You must know the Ethernet address of the Gateway.
- You must know the Unit ID of the ZBRN32 access point.
NOTE: Each ZBRN32 access point needs a mid-range device license in PME.
- You must know the temperature sensor locations on the busway to be able to assign meaningful names to the equivalent sources in PME.