Thermal Monitoring of Medium Voltage (MV) Substations
Overview
This application provides remote, continuous monitoring of the thermal conditions of MV substations equipped with Easergy TH110 temperature sensors and Easergy CL110 environmental sensors. Thermal monitoring can help you find exceptional conditions in the substation equipment, such as overloads or faulty power connections of cables, busbars, circuit breakers, or transformers. In addition, this application can monitor the environmental conditions, ambient temperature and humidity, inside the substation and switchgear cubicles. You can see temperature data in real-time, analyze historical trends, and receive alarms and notifications. Any applicable PME power monitoring features can be used with the substation monitoring data.
For more information on the value of Continuous Thermal Monitoring see the EcoStruxure Power Digital Applications for Large Buildings & Critical Facilities Design Guide. See Resources for download information.
                                                     warning
warning
inaccurate data results
| ● | Do not incorrectly configure the software or the devices. | 
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. | 
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. | 
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. | 
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
NOTE: The examples and screen captures shown in this application description are for illustration purposes only. They are not intended to give guidance on configuration settings or application details. For guidance on configuration of your system or other application details, consult a qualified professional.
Examples:
                                                 
                                                
                                            
The above is an example of a real-time trend showing cubicle and transformer temperature and humidity measurements over the last hour.
                                                 
                                                
                                            
The above is an example of a trend report showing a 1-week cubicle temperature trend.
                                                 
                                            
The above is an example of an alarm status view showing thermal monitoring related alarms.