Prerequisites

The following is required to set up the Thermal Monitoring of MV Substations application in PME:

  • PME 2023 must be installed and commissioned.
  • The TH110 and CL110 sensors, the ZBRN32 access points, and the SMDs in the substation must be configured, connected, and communicating.

    NOTE: This application supports SMD v4.0 and v3.0. SMD v2.0 is not supported.

  • The SMDs must be accessible from the PME server by Ethernet.
  • You must know the IP address of the SMDs.

    NOTE: Each SMD needs a mid-range device license in PME.