4. Integrating PME Web applications in Building Operation
Integrating PME Web applications in Building Operation includes the following steps:
- Configuring Dashboard, Diagrams, Trends, Alarms, Reports, and EWS measurements and generate the import file with the web application Integration Utility settings.
- Importing the configuration file into Building Operation
- Setting up EWS credentials in PME (server) and Building Operation (client)
- Enabling embedded content in PME and Building Operation
See the following sections for details.