Updating the EWS Server
After adding the devices or making any changes to the device configuration in the PME, you must update the EWS server through the Update EWS Server tool in the Management Console.
NOTE: Run Management Console as Administrator user. To do this, right-click the Management Console program icon and select Run as administrator from the context menu. If you do not run it as Administrator, then certain tools such as Update EWS Server are not functional.
To update EWS Server:
- Open Management Console.
- Select Tools > System > Update EWS Server. A dialog box appears indicating that the update to the EWS server configuration was successful.
- Click OK when the Update EWS Server confirmation dialog appears.