Solution Limitations

Only the PME Standalone Architecture installation type, where the PME application server and the database server are installed on the same computer, is supported by the PME/EBO Integration solution. The PME Distributed Database architecture installation type is not supported. See System architecture for more information on PME installation architectures.