Configuring PME server settings
Install a security certificate for TLS 1.2
PME uses Transport Layer Security (TLS) 1.2 for an encrypted, authenticated connection using HTTPS between the server and the Web clients.
A security certificate must be installed on the PME server and must be bound to the Default Web Site, which is used by PME. By default, if no bound certificate is detected, PME is installed with a self-signed certificate.
RECOMMENDATION: We strongly recommend that you replace the self-signed certificate with an authority issued certificate.
Set SQL Server memory options
Set the SQL Server memory options to optimize system performance.
NOTE: Setting the SQL Server memory options applies only to full, standard editions of SQL Server. It does not apply to SQL Server Express editions.
See Setting SQL Server memory options for details.