Computer Hardware

The performance of a computer is determined by the following factors:

  • Computer type (desktop, workstation, or server)
  • Central processing unit (CPU)
  • Random-access memory (RAM)
  • Data storage, for example Hard Disk Drive (HDD)

When choosing the computer hardware for your PME system, you need to consider the following:

  • Number of devices in the system
  • Number of concurrent users
  • System performance expectations
  • Data exchange with other systems
  • Historical data logging needs
  • System availability and recovery needs

NOTE: Undersized computer hardware is a common source of performance issues with PME systems.