Choosing Computer Type, CPU, and RAM
The computer type, CPU, and RAM determine the overall performance and reliability of the system. CPU is important for device communications and RAM affects SQL Server performance.
As a starting point for the selection of these components, we are defining two different system categories, Basic Systems and Advanced Systems. Decide which category best describes your system needs and then use the information provided in the tables below to define your computer hardware specifications.