Operating System considerations
Windows or Windows Server?
PME supports both Windows and Windows Server operating systems. However, we recommend you use the Windows Server for the following reasons:
- Windows Server can use server-class computer hardware. It can access more CPUs and more RAM than Windows. For example, Windows 10 is limited to two physical CPUs.
- Windows Server offers better performance for running PME services.
32-bit or 64-bit systems?
PME supports 64-bit operating systems only.