Before upgrading the software
Review the prerequisites
Before starting the upgrade,
Backup the databases
Backup the ION_Data, ION_Network, ION_SystemLog, and ApplicationModules databases before starting the upgrade. Keep the backups in a secure and safe location. Use these backups to restore the original databases in case data is deleted or lost, accidentally, during the upgrade.
notice
LOSS of data
| ● | Back up the database at regular intervals. |
| ● | Back up the database before upgrading or migrating the system. |
| ● | Back up the database before trimming it. |
| ● | Back up the database before making manual database edits. |
| ● | Verify correct database behavior after making database or system changes. |
Failure to follow these instructions can result in permanent loss of data.
Cybersecurity
Review the cybersecurity information. See Cybersecurity for details.
Upgrade Path
An upgrade path describes from which older system to which newer system PME is upgraded. There are many possible upgrade paths, but only some are supported by the In-Place and Side-by-Side upgrade tools and procedures. See Determine your upgrade path for information on how to determine your upgrade path.
Upgrade Type
There are two different upgrade types, In-Place Upgrade and Side-by-Side (SBS) Upgrade. Each type uses different tools and has different prerequisites. See Determine the upgrade type for information on upgrade types.
Service Packs
The In-Place and SBS upgrade tools require the latest service pack versions of the older PME systems to be installed before the upgrade. For example,
Your upgrade path determines if your old system requires a service pack installation before the upgrade. See Determine your upgrade path for more information. See Upgrade tools and resources for information on where to get the latest service packs for older versions of PME.
Operating Environment
A requirement for in-place upgrades is that the Operating System and Database Server versions are supported by the new PME system.
Licensing
Product licensing might have changed between the old version of PME and the new version. Review Licensing and in particular Important notes on licensing for more information, and make sure you have the correct licenses for the new system before starting the upgrade.
Windows Integrated Authentication for SQL Server
If you are planning to upgrade PME to use Windows Integrated Authentication, then complete the following before starting the upgrade:
NOTE: Windows Integrated Authentication is not supported for PME systems with Secondary Servers.
Standalone architecture
On the PME application server:
- Add the Windows account for the user who is upgrading the software to the local Administrator group.
- Add the Windows account for the upgrade user to the SQL database logins with a sysadmin Server Role.
NOTE: You can remove this account from the SQL database logins after PME is upgraded.
- Add the Windows account that is used by PME to access the databases to the local Administrator group.
- Set the 'Logon As A Service' privilege for the database access account.
Distributed Database architecture
On the Windows Domain, in the Active Directory:
- Add an account for the user who is upgrading PME. This only needs to be a domain user account, not a domain admin account.
- Add an account that PME will use to access the databases. This only needs to be a domain user account, not a domain admin account.
On the PME application server:
- Add the account for the upgrade user to the local Administrator group.
- Add the database access account for PME to the local Administrator group.
- Set the 'Logon As A Service' privileges for the database access account.
On the database server:
- Add the account for the upgrade user to the local Administrator group.
- Add the account for the upgrade user to the SQL database logins with a sysadmin Server Role.
NOTE: You can remove this account from the SQL database logins after PME is upgraded.
NOTE: When PME is installed with Windows Integrated Authentication, the Windows account that is used to access the database is also used to run the PME services and the IIS Application Pools.
Upgrade troubleshooting
Rolling back an unsuccessful PME in-place upgrade
Under certain circumstances the database upgrades, which are part of the system upgrade, might not be successful. Use the following steps to rollback an upgrade where the database upgrades were not successful. After completing these steps, your system should be back in the state it was in before the upgrade.
To rollback an in-place upgrade with unsuccessful database upgrades:
- Close the PME installer.
- Restore the PME databases from backup, using Microsoft SQL Server Management Studio.
NOTE: Backing up the databases was an optional, recommended step in the in-place upgrade workflow of the software installer.
- Open the Windows Service panel and start all ION services. Also, re-enable and start the Application Modules services as follows:
NOTE: The installer stopped the ION services and disabled the Application Module services during the upgrade.
- ION Application Modules Alarm Service Host (Startup Type = Manual)
- ION Application Modules Core Services Host (Startup Type = Automatic)
- ION Applications Modules Data Services Host (Startup Type = Automatic)
- ION Applications Modules Provider Engine Host (Startup Type = Automatic)
- Open Internet Information Services Manager (IIS Manager) and start the PME application pools:
- Application Modules AppPool
- ION AppPool
- WebReporterAppPool
- Verify that the system is operating as expected.