PME Services
Configuration Manager does not transfer customizations in services settings from the source to the target.
Recreate PME Services settings customizations in service settings using Microsoft Windows Services.
Additionally, custom VIPs need to be manually started after Configuration Manager completes the Write to System and the system is ready to be put into service.