Web Application web.config
Configuration Manager does not automatically install the source system web.config
file on the target system because there could settings in the file that are incompatible between source and target system.
To recreate web.config
customizations:
- In the
CM Migration Files
folder, check the copiedweb.config
file and compare it to the target system defaultweb.config
file in...\Applications\SystemDataService\
. - Back up
web.config
on the target system and then edit the file as needed.
NOTE: You must reconfigure the system after editing the Web Applications web.config file. That means you have to return to Step 3 - Initialize the Configuration in the workflow.