System Log events
System Log Events lists events for components in the system. This information comes from the ION_SystemLog database.
TIP: For instructions on filtering and sorting columns and customizing the display, see Customizing and navigating interface displays.
Viewing System Log events
To view System Log Events:
- Select System Log Events from the System Setup pane.
-
In the Show area select the checkboxes for the system components for which you want to view events (i.e., servers, sites, devices).
If there are no events for a particular system component, that check box is unavailable.
- Select the minimum priority level of events to be displayed from the Minimum Priority Level dropdown list (see below for more information on priority levels).
- Click Modify to change the date/time filter applied to the System Events Log display. See System Log filter setup.
- To view details of an event, double-click on the entry in the event log.
Priority
Priority classifies what type of event has occurred. The value corresponds to the severity of the event: the higher the number, the more severe the event.
The priority is contained in the ION_SystemLog database as a number. In the System Events Log display, the priority levels are displayed as text strings. The priority numbers are mapped to the text strings as follows:
| Diagnostic | 0 - 5 |
| Information | 6 - 20 |
| Warning | 21 - 63 |
| Error | 64 - 191 |
| Critical | 192 - 255 |
By default, the Cutoff setup register of Log Inserter’s System Log Controller module is set to 192. This means that system events with a priority less than 192 are not transferred to the ION_Data database and therefore cannot be viewed in Alarms. If you want to view lower priority events in Alarms, use the above priority mapping as a guide to set the Cutoff setup register to a lower value (using Designer).
System Log filter setup
The System Log Filter Setup dialog lets you change the date and time filter applied to the System Events Log display.
- Click Modify to display the System Log Filter Setup dialog.
- Select the time range by which you want to filter from the dropdown list. To set up a custom filter, select Custom Date Range then use the dropdown lists and arrows in the Select a Date Range dialog to specify the start and end of the range.
- Click OK.