Update OPC Server

Use this function to initialize or update the OPC measurement mappings in the system. This function is part of the OPC server capabilities of PME. For information on how to map ION registers to OPC, see OPC DA measurement support. For information on how to map Modbus registers to OPC, see Device Type Editor.