Creating new measurements

You can use Manual Data Editor to create new, custom measurements in PME. These measurements are available anywhere in the software.

To create a new measurement:

  1. In Manual Data Editor, click Load New Data to open the Load Data dialog box.

    NOTE: Load Data opens automatically when you start Manual Data Editor.

  2. In Load Data, click Create new Measurement to open the Create new Measurement dialog box.

    NOTE: Check the list of available measurements to see if one exists for your application before creating a new measurement.

  3. In Create new Measurement, enter the relevant information for the new measurement.
  4. Click Create to add the new measurement to the system.
  5. (Optional) Repeat steps 2-4 to add additional measurements.
  6. Close Manual Data Editor.

 

For information on how to use the Manual Data Editor , see:

For reference information see: