OPC DA Server Support
Introduction to OPC
OPC is a set of open standards for connectivity and interoperability of industrial automation and the enterprise system. OPC provides a bridge between Windows based applications and process control hardware, thereby eliminating the need for proprietary or custom interfaces and drivers for the various data types and sources residing in your corporate information network. Having information readily available in a universally-recognized format can cut costs, speed up development and increase operations efficiency. This is especially true when many diverse software applications, hardware, and operating systems exist in the corporate and operations networks.
RECOMMENDATION: Use an OPC tunneling application for OPC DA data exchange over a network
warning
inaccurate data results
| ● | Do not incorrectly configure the OPC Server. |
| ● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
| ● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
OPC DA is supported through the implementation of
Power Monitoring Expert supports OPC DA server and OPC DA client functionality. The OPC DA server translates ION data into OPC DA data, for exporting and viewing in other third-party OPC DA client systems. The OPC DA client, on the other hand, takes OPC standardized measurements from third-party systems and translates them into a data format that Power Monitoring Expert can use.
This appendix provides basic configuration and operation instructions for the OPC DA server component of Power Monitoring Expert.
NOTE: The OPC DA client is available in all Power Monitoring Expert installations. However, due to the number of different third-party OPC DA - compliant servers in the industry, as well as different methods and syntax for connecting to these servers and accessing their data, it is highly recommended that you contact Technical Support for assistance in configuring the OPC DA client.
Optional OPC DA server license
The OPC DA Server Assistant is available during the 90-day trial period. After the trial period, you need to purchase a Data Exchange Module license and activate it through the License Configuration Tool to enable OPC DA server functionality.
OPC DA server type
The Power Monitoring Expert OPC server complies with the "OPC Data Access Custom Interface Standard Version 2.05A". The class of data that the current release of OPC DA Data Access server is able to provide is Read-Only data (i.e., control functions are not currently supported).