Test the PME OPC UA client configuration in Vista

  1. Open Vista using your PME credentials.

  2. Drag and drop a Numeric Object to the workspace.

  3. Right-click the Numeric Object and then select Link.

  4. Select Custom and then select Edit Link.

  5. Select the correct Nodes, Managers, Modules, Output Registers and then select OK.

    You can see the real time data through on the PME OPC UA server through PME OPC UA client.

  6. Select File > Save to save the Vista file.

  7. Log in to PME web.

  8. Go to Diagrams and select the file name saved in Vista.

    The Network Diagram screen appears.