Configure the Power Losses Report
warning
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
To configure the Power Losses Report,
- Set up the monitoring devices that record the input and output data for the transformers and UPS. See Supported Measurements and Devices for details on which measurements are required.
- Define the power losses system using the Power Losses Configuration Utility.
- Open the report template in the Reports Web Application, set the report input parameters, and generate the report.
For information on how to use the report, see Power Losses Report.