(Optional) Create a Power Quality Performance link in the Web Applications

An optional step is to create a link in Web Applications to view the Power Quality Performance Vista diagrams:

See Customizing the Web Applications links for details on how to create this link. See Adding idle detection to custom Web Application links for information on how to add idle detection to prevent session timeouts.