Assigning engine data
The Assign Engine Data Measurements editor is used to map PME engine measurements to engine data that is recorded by a monitoring device for the generator engine.
To assign engine data:
- Click Assign Engine Data to open the Assign Engine Data Measurement editor.
- Click New to add a new assignment. Complete the following fields:
- Engine Data Measurement - Select the measurement you want to assign.
- Source - Select the monitoring device that records the engine data of the generator.
- Measurement - Select the monitoring device data that you want to map to the engine measurement.
- (Optional) Repeat step 2 to map additional measurements.
- Click OK to save the measurement mapping and close the Edit Engine Data Measurements window.
TIP: See Editing Engine Data for information on how to define engine measurements.