Define Equipment
Use the Equipment tab to add new Equipment or edit existing ones. An Equipment represents a real life apparatus such as a piece of switch gear, or a distribution panel. You can map the Equipment to a measurement and rating. Equipment can be added to a Group and be included in the reports.
You can perform the following actions on this tab:
- Click New to add a new Equipment to the system. See Adding Equipment for details.
- Click Clone to add a copy of an existing Equipment. The tool copies many of the existing device settings into the new entry. You can then enter the unique details of the new device.
- Click Delete to remove records from the system.
- Click Revert (before you click Apply or OK) if you make changes to a record and want to revert to your initial settings.