UPS Power Configuration Utility
TIP: You can open the UPS Power Configuration Tool from the Power Monitoring Expert > Configuration Tools folder on your desktop.
Use the UPS Power Configuration Utility to configure the Capacity Management Module. With this tool you define UPS Systems for the UPS Power Report.
Prerequisites
- The monitoring devices that are recording the UPS data must be configured in the PME Management Console and must be communicating before you can configure the components and properties in the configuration tool.
User Interface
| Control | Description |
|---|---|
| Help | Opens the help for the utility. |
| New | Creates a new entry in the grid. |
| Delete | Deletes the selected entry from the grid. |
| OK | Saves all changes and exits the utility. |
| Cancel | Exits the utility without saving changes. |
| Apply | Saves all changes and leaves the utility open. |
| Grid Area Columns | Description |
|---|---|
| Modified | Displays a status symbol for the record. |
| + (plus) | A new entry. |
| * (asterisk) | An existing entry has been modified. |
| ! (exclamation mark) | The entry is incorrect. |
| System | Displays the system name. |
| Type | Displays the UPS system type (N, 2N, N+2, etc.) |
| Description | Displays a description of the system |
TIP: The tool indicates if there configuration errors. Point at the red exclamation icon
to see configuration error details.