TGML performance
| Number of devices | Graphics Editor TGML Category type | Total number of Graphics Editor TGML Category Type (Components) | PME Web Application Average Response Time (seconds) |
|---|---|---|---|
| 5 | Components (Component library) | 50 | <1 |
| 10 | Components (Component library) | 100 | <2 |
| 50 | Components (Component library) | 200 | <3 |
Graphics Editor TGML: 5 tabs currently open on single client (Each tab bind with 500 measurements)
| Number of devices | Graphics Editor TGML Category type | Total number of Graphics Editor TGML Category Type (Tabs Snippet) | PME Web Application Average Response Time (seconds) |
|---|---|---|---|
| 5 | Tabs (Web Applications) | 1 | <5 |
| 10 | Tabs (Web Applications) | 5 | <10 |
For Graphic Editor
-
If a meter is secured with advanced security mode, the Sources, Modules, Managers and Registers take more time to load during the initial Configuration step.
-
For Meters with Firmware V4.5 and has Advanced Security and Legacy security support enabled, the Meter Password should be set as Non-Zero. Also, the Username is not editable, it is Default always.