Configuring a transformer

To configure a transformer that you added to a one-line in the Graphics Editor:

  1. Edit the following Exposed Properties:
    • BaseColor: Set the color of the selected component to change the color of the entire component.
    • StrokeWidth: Set the stroke width for the entire component that is selected.