Report Theme
Change the Report theme to customize the Reports colors and the Reports logo.
To change the Reports colors:
- Under Report Colors, select Use Theme Colors or Override Theme Colors.
TIP: The system theme colors are defined by the System Theme settings for the Web Applications. See System Theme for more information.
- If you choose Override Theme Colors, then set the colors for the Report Title, Section Header, Table Header, Summary, Row Shading, and Section Title, using the drop-down selectors.
- Click Save to apply the changed settings.
To change the Reports Logo:
- In SETTINGS, open the Settings Library and click Report Theme.
- Under Report Logo, click Select to open the Select Report Logo Image dialog.
- Select an image currently available in the repository, or
- Click Upload Image to choose an image file available on your system or drag an image file into the application area.
- Click Finish to add it to the image repository.
- Click OK to complete your selection.
- Click Save to apply the changed settings.
NOTE: You can use GIF, JPG, JPEG, or PNG image formats. The recommended file size is 250 x 100 pixels. Images are automatically re-sized to fit the logo area in Reports.