Session Timeout
Use the session timeout settings to define the timeout behavior of the software web applications and Windows applications clients.
You have to following options:
- You can enable and set a timeout for the web applications.
- You can enable and set a timeout for the Windows applications.
NOTE: You can enter a timeout value from 1 minute to 1440 minutes (1 day)
When a session timeout is configured, web application clients are logged out and Windows application clients (Vista, Designer, Management Console) are locked after a period of inactivity. The default timeout for both client types is 20 minutes. To restart or unlock the session you must enter the login credentials.
A session is considered inactive when none of the following actions are detected for the duration of the timeout period:
- Mouse movement
- Mouse clicks
- Keyboard activity
- Touch screen activity