UPS Auto Test Report
NOTE: This report is part of the Backup Power Module. This module requires a separate license.
Summary
The UPS Auto Test Report shows test information for UPS systems, such as test times, pass/fail evaluation, and event logs. Use this report to assess the performance of your UPS systems during test runs.
NOTE: You can only use this report with certain types of UPS systems. See Backup Power Module configuration for details.
Prerequisites
- The Backup Power Module must be configured.
- The measurement data must be available as historical data logs in the database.
Report inputs:

Type a title for the report in the text box.

Add the UPS groups that you want to include in the report.

Use this input to select the timeframe for the data you want to view in the report.
Select the reporting period from the dropdown list. The timeframe options in the timeframe dropdown are relative to the date the report is run. To run a report that starts and ends in the past, select the fixed date option. Type a start and end date in the date boxes or click the arrows beside the dates to display a pop-up calendar and select a date. Type a time in the time boxes or click the up and down arrows beside the time to adjust the hours or minutes up or down. You can also run a report that starts and ends in the future. You must manually add the future data. You can use any tool to generate future data. For example, use Manual Data Editor to manually enter measurement data.
Select the timezone you want to view timestamps in.

Click Yes to include event log data in the report. Click No to exclude it.

Click Yes to include data warnings in the report. Click No to exclude them.
Example:
NOTE: This example only shows selected content from the report, it does not show the entire report.