Circuit Breaker Aging Report
NOTE: This report is part of the Breaker Performance Module. This Module requires a separate license.
Summary
The Circuit Breaker Aging Report shows the aging and wear related status of circuit breakers. Use this report to check the condition of your breakers and to plan preventive maintenance.
Prerequisites
- The Breaker Performance Module must be configured.
- The measurement data must be available as historical data logs in the database.
Report inputs:

Type a title for the report in the text box.

Select the group for which the report is intended.

Select from the dropdown list to determine how the circuit breaker aging and electrical wear analysis results are sorted.

Select Yes or No. Selecting Yes allows all of the breakers to appear in the report regardless of the current electrical aging and electrical wear levels. Selecting No allows only breakers with moderate or critical electrical aging and electrical wear to appear.

Click Yes to include data notifications in the report. If there are none, the section is not included. Click No to exclude this section.
Example:
NOTE: This example only shows selected content from the report, it does not show the entire report.