Device Replacement Report
Summary
The Device Replacement Report shows the device last replacement date and the next date for replacement. Use this report to understand and manage your device replacement operation.
Prerequisites
- The device must be configured in the Device Replacement Manager.
Report Inputs

Type a title for the report in the text box.

Use this input to select the timeframe for the data you want to view in the report.
Select the reporting period from the dropdown list. The timeframe options in the timeframe dropdown are relative to the date the report is run. To run a report that starts and ends in the past, select the fixed date option. Type a start and end date in the date boxes or click the arrows beside the dates to display a pop-up calendar and select a date. Type a time in the time boxes or click the up and down arrows beside the time to adjust the hours or minutes up or down. You can also run a report that starts and ends in the future. You must manually add the future data. You can use any tool to generate future data. For example, use Manual Data Editor to manually enter measurement data.
Select the timezone you want to view timestamps in.
Example:
NOTE: This example only shows selected content from the report, it does not show the entire report.