Measurement Aggregation Report
Summary

The Measurement Aggregation Report gives aggregated logged measurement data in tabular format. The aggregation intervals are configurable, and the report supports aggregation by time of use. Use this report to understand the consumption patterns of your facility or processes.

Prerequisites
  • The measurement data must be available as historical data logs in the database.
Report inputs
Example 1 - Report output with Rollup set to Interval:
Example 2 - Report output with Rollup set to Hour:

NOTE: This example only shows selected content from the report, it does not show the entire report.