Transform task: Setting parameters and recommended values
Transform task settings
Setting Name |
Description |
Setting Parameters / Recommended Values |
---|---|---|
Transform |
||
Intervalization Method |
Specifies the method used when converting the values from an irregular interval into a regular interval. |
Use default 'Last Known Value' setting |
Intervalize to present time |
When set to True, the data is intervalized up to the current system time. If set to false, the data is intervalized up to the most recent data point. |
Set value to “False” |
Target Reading Interval (minutes) |
Data is intervalized to a reading interval specified in this field. |
Interval value in minutes. Select a value from the dropdown list. Default value of 15 minutes is suitable in most cases. |