Supported measurements and devices
The following measurements have been pre-mapped in the Sample WAGES rate file:
Power
| Measurement | Unit | ION Name |
|---|---|---|
| Block Demand Apparent Power Total | kVA | Apparent Power Sliding Window Demand Delivered+Received |
| Block Demand Reactive Power | kvar | Reactive Power Sliding Window Demand Delivered - Received |
| Block Demand Active Power | kW | Active Power Sliding Window Demand Delivered-Received |
Energy
| Measurement | Unit | ION Name |
|---|---|---|
| Apparent Energy Total | kVAh | Apparent Energy Delivered + Received |
| Reactive Energy Into the Load | kvarh | Reactive Energy Delivered |
| Active Energy Into the Load | kWh | Active Energy Delivered |
The Energy by IT Customer Report supports the measurements listed in the tables below. Only one measurement of each type (Energy , Current) is required. If multiple types of the same measurement exist in the system, then a look-up method is used to determine which one to use. The tables list the supported types in order of look-up priority.
NOTE: You can edit this list of measurements in the PME database.
Energy
| Measurement | Unit | ION Name | ION Label |
|---|---|---|---|
| Active Energy | kWh | Active Energy Delivered – Received | kWh del-rec |
| Active Energy Into the Load | kWh | Active Energy Delivered | Active Energy Delivered |
Current
| Measurement | Unit | ION Name | ION Label |
|---|---|---|---|
| Current Average Mean | A | Current Phase Average Mean | I avg mean |
| Block Demand Current Avg Into the Load | A | Current Phase Average Sliding Window Demand Delivered | Amps Avg Dmd |
| Current Avg | A | Current Phase Average | Current Avg |
The following devices can provide the measurements required for this report:
- BCPM-E, PM5350 (multi-circuit mode)
- Basic, Intermediate, or Advanced Device for main service entrance (PM5xxx, PM8xxx, ION7650, ION9000)