EPSS Transfer Time alarm

The ATS and generator status changes trigger general Backup Power Asset Monitoring alarms in PME, if the correct status labels are used. See Configure Generator Test EPSS for details. You can also configure the system to show a Transfer Time Asset Monitoring alarm, including EPSS transfer time details, for a test run or a real backup power supply incident. To set up such an alarm, you need to create a setpoint on the device monitoring the ATS status that is triggered by the Test, Power Outage, and Emergency status signals. The setpoint must use the label: Transfer Time for the module name and the setpoint status output register.

The following shows an example ION framework to create a Transfer Time alarm in PME: