Supported measurements and devices

The Branch Circuit Power Report needs branch circuit level measurements. It supports the measurements listed in the tables below. Only one measurement of each type (Demand, Current) is required. If multiple types of the same measurement exist in the system, then a look-up method is used to determine which one to use. The tables list the supported types in order of look-up priority.

NOTE: You can edit this list of measurements in the PME database.

Demand/Power
Measurement Unit ION Name ION Label
Block Demand Active Power kW Active Power Sliding Window Demand Delivered-Received Demand Real Power
Block Demand Active Power Into The Load kW Active Power Sliding Window Demand Delivered kW sd del
Active Power Mean kW Active Power Mean kW tot mean
Active Power kW Active Power kW tot
Current
Measurement Unit ION Name ION Label
Current Average Mean A Current Phase Average Mean I avg mean
Block Demand Current Avg Into the Load A Current Phase Average Sliding Window Demand Delivered Amps Avg Dmd
Current Avg A Current Phase Average Current Avg

The following devices can provide the measurements required for this report:

  • BCPM-E
  • PM5350 (multi-circuit mode)