Supported measurements and devices
The report and Vista diagrams in the Insulation Monitoring Module support the following measurements and devices:
Standard | Input Measurements | Suitable Devices |
---|---|---|
ANSI |
Total Hazard Current (THC)
|
Iso-Gard Series 6 Line Isolation Monitor (Schneider Electric device) |
IEC |
Insulation Resistance (Ohm)
|
Vigilohm IM20 (Insulation Monitor) |