Required measurements for Power Quality Performance monitoring
The following table shows which measurements are required for the different Power Quality Performance components:
NOTE: For each disturbance category, choose only the needed measurements from the supported list to log. Do NOT Log all of them. Logging all measurements can cause unwanted database growth, and performance issues.
| PQ Disturbances | Used by | Supported Measurements | Label Name |
|---|---|---|---|
|
Voltage Unbalance |
PQ Performance Diagrams |
ION Devices |
V unbal mean |
|
Non-ION Devices |
Voltage Unbalance L-L Worst |
||
|
Current Unbalance |
PQ Performance Diagrams |
Non-ION Devices |
Current Unbalance Worst |
|
Voltage Harmonics |
PQ Performance Diagrams |
ION Devices |
V1 Total HD1 |
|
Non-ION Devices |
THD Voltage A-B |
||
|
Current Harmonics |
PQ Performance Diagrams |
ION Devices |
I1 Total HD1 |
|
Non-ION Devices |
THD Current A |
||
|
Frequency Variation |
PQ Performance Diagrams |
ION Devices |
Freq mean |
|
Flicker |
PQ Performance Diagrams |
ION Devices |
V1-Flck Plt |
NOTE: 1 Use only for ION 6200, 7300, 8600C, 8650C and 8800C. These measurements are NOT logged by default.
NOTE:
- PM8000 is categorized as an ION device.
- ION6200 is categorized as a non-ION device.