Access Denied Errors
Issue: When I try to view real time values in my Vista diagram on my target machine I get an access denied message when I hover over a register:
                                             
                                        
Likely cause: The meter security settings were enabled and set on the source system.
Resolution: On the target system, open Management Console, select Devices, right-click the device and then select Security. In the Meter Security Settings dialog, enter the correct security settings for the device.
NOTE: A similar error occurs if the server, sites, or devices are not enabled after the configuration is written to a system, or if the Ethernet is not connected.