PME 2024 Install notes
The following is a list of release notes related to
- Install path length limitation
- 32-bit version of SQL Server Express is not included with the PME installer
- Install a security certificate for TLS 1.2
Install path length limitation
The installation path for installing PME on your computer is limited to 100 characters. This is done to ensure that the path length of PME system files, after the installation, does not exceed the maximum allowable path length of 260 characters. This maximum path length is a limitation on some of the older supported Windows operating system versions.
32-bit version of SQL Server Express is not included with the PME installer
32-bit versions of SQL Server Express are still supported, but they are not included with the installer. If you want to use a 32-bit version, you need to install it on the PME server before installing the software.
The 64-bit version of SQL Server Express is included with the installer and can be installed as part of the PME installation workflow.
Install a security certificate for TLS 1.2
See Install a security certificate for TLS 1.2 in the Install section of this guide for details.