Alarm to incident mapping
The following table shows the mapping of alarm types to Incidents:
| Incident Category | Incident Type | Alarm Types | 
|---|---|---|
| Power Quality | Interruption | Interruption | 
| Over Voltage | Over Voltage | |
| Under Voltage | Under Voltage | |
| Unclassified Disturbance | Unclassified Disturbance | |
| Sag | Sag (Voltage) | |
| Swell | Swell (Voltage) | |
| Transient | Transient | |
| Flicker | Flicker | |
| Frequency Variation | Frequency Variation | |
| Harmonics | Harmonics | |
| Harmonics (Current) | ||
| Harmonics (Power) | ||
| Harmonics (Voltage) | ||
| Unbalance | Unbalance | |
| Unbalance (Current) | ||
| Unbalance (Voltage) | ||
| Diagnostics | Communication Status | Communication Status | 
| Device Status | Device Status | |
| System Status | System Status | |
| Energy Management | Air | Air | 
| Demand | Demand | |
| Electricity | Electricity | |
| Gas | Gas | |
| Power Factor | Power Factor | |
| Steam | Steam | |
| Water | Water | |
| Asset Monitoring | Arc Flash | Arc Flash | 
| Backup Power | Backup Power | |
| Current Monitor | Over Current | |
| Sag (Current) | ||
| Swell (Current) | ||
| Under Current | ||
| Protection | Protection | |
| Thermal Monitor | Thermal Monitor | |
| General | Clutter | General Event | 
| Clock / Time | ||
| Device Settings | ||
| Unassociated Dropout | ||
| General Setpoints | General Setpoint |