Device Replacement user interface
Main user interface (UI)
Main UI
| 1 |
Help
|
| 2 | Selection tabs
Select a tab to see information related to Device Replacement or Processed Measurement. |
| 6 | Number of displayed items
Shows the number of items visible on this page, and the total number in the system. |
| 7 | Page Selector
Use the page Selector to navigate between pages of information. Set the number of items that are displayed on a page. |
Device Replacement tab
| 3 | Search Devices box.
Enter a search string to find devices in the devices replacement table. |
| 4 | Date Range Filter.
Use the date range filter to customize which devices are displayed in the devices replacement table. |
| 5 |
Devices replacement table
|
Processed measurement tab
| 1 |
Create
|
| 2 |
Processed measurement table
|