Add Recipient UI

1

Recipient details

The recipient name, email address, phone number (used for SMS messaging), and SNMP server name. Email, phone number, and SNMP server name are optional; however they are needed if email, SMS, or SNMP notifications should be sent to this recipient.

NOTE: Enter the phone number in E.164 number formatting: [+][country code][area code][local phone number]. Example: +14151231234.

2

Address test

Select the Test button for the address (email, phone number, or SNMP server name) you want to test. An address test will send a test message to the email address or phone number configured in the recipient details.