Automated measurement mapping of EWS Client

EWS server measurement name is automatically mapped to PME measurement name based on the following scenarios:

  • Full Name Match: The complete EWS server measurement name matches 100% with the PME measurement name.

    For example: If EWS server measurement name is "Active Power", this name is 100% match with the PME name "Active Power", then this EWS server measurement is automatically mapped to "Active Power" of PME measurement.

  • No Name Match: No part of the EWS server measurement name 100% matches with the PME measurement name.

    For example: If EWS server measurement name is "Power", this complete name is not 100% match with PME measurement name nor contains 100% match with PME measurement name, then this EWS server measurement is not automatically mapped. This measurement should be manually mapped.