Additional Advanced Reporting and Dashboards Modules component
Additional software modules compatible with the Advanced Reporting and Dashboards Module are included on the Power Operation installation media and can be optionally licensed with Power Operation. These modules address a variety of electrical network, asset, and energy management needs.
Licensing options
Each module is licensed individually and requires at least one Advanced Reporting and Dashboards license. For more information on licensing, see License keys.
You can license the following software modules on the same system as the Advanced Reporting and Dashboards Module using the License Configuration Tool:
Commercial reference | Software module |
---|---|
PSA104112 | Advanced Reporting and Dashboards Module |
PSA104114 | Energy Billing Module |
PSA104115 | Breaker Performance Module |
PSA104116 | Energy Analysis Reports Module |
PSA104121 | Capacity Management Module |
PSA104124 | Power Quality Performance Module |
PSA104125 | Insulation Monitoring Module |
PSA104126 | Backup Power Module |
PSA104130 | Energy Analysis Dashboards Module |
For more information on licensing software modules, see Activating software module licenses.
Design considerations
See Integrating with Advanced Reporting and Dashboards for details.