Additional Advanced Reporting and Dashboards Modules component

Additional software modules compatible with the Advanced Reporting and Dashboards Module are included on the Power Operation installation media and can be optionally licensed with Power Operation. These modules address a variety of electrical network, asset, and energy management needs.

Licensing options

Each module is licensed individually and requires at least one Advanced Reporting and Dashboards license. For more information on licensing, see License keys.

You can license the following software modules on the same system as the Advanced Reporting and Dashboards Module using the License Configuration Tool:

Commercial reference Software module
PSA104112 Advanced Reporting and Dashboards Module
PSA104114 Energy Billing Module
PSA104115 Breaker Performance Module
PSA104116 Energy Analysis Reports Module
PSA104121 Capacity Management Module
PSA104124 Power Quality Performance Module
PSA104125 Insulation Monitoring Module
PSA104126 Backup Power Module
PSA104130 Energy Analysis Dashboards Module

For more information on licensing software modules, see Activating software module licenses.

Design considerations

See Integrating with Advanced Reporting and Dashboards for details.